9/16/2013 11:25 AM | |
Joined: 4/25/2011 Last visit: 6/29/2024 Posts: 128 Rating: (5) |
Dear Expert's In my project i have 315-2DP CPU and X number of breakers which are already in line. but now i want to change profibus address for one breaker. HW Configuration showing ???? in connected DP device as attached file. How can i get actual configuration, what are the requirement for same. i have already download GSD file and install but problem remains same. Thanks & Regard's Attachmentimages.zip (225 Downloads) |
Naveen Paliwal |
|
9/18/2013 11:28 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi In image 1 what is written in Optional pack ...? Did you miss that software? SENTRON_WL_VL_communication__PROFIBUS_EN.pdf |
Last edited by: Ste39 at: 9/18/2013 11:38 AM |
|
9/19/2013 8:57 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello Which version of STEP 7 you have installed? you can send us the full code of 3WL? |
Follow us on