10/7/2015 8:12 AM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating: (936) |
Regarding the button, I suggest using APL template, by using the APL operator button 1. Copy the APL_OP_BUTTON from @PCS7_ElementsAPL.pdl. 2. Assign a meaningfull name to your object 3. Enter your object name in the "stUser" object 4.At the OpAreaHeading property you can set three of five button operation, by using @pg_apl_oa_binary103.pdl (three) or @pg_apl_oa_binary105.pdl (five). 5. Adjust your object by using the following properties.
For the rest: I don't think you can set something in CFC block without using OCM through WinCC.. The only other way is to use a digital operation signal (OpDI) with OCM and connect the output to your block. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
1/2/2016 8:52 AM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating: (195) |
New question published by IT service is split to a separate thread with the subject PCS7 - stucked with very simple (I think) but valuable issue. Best regards |
My Forum is the place to personalize your profile, |
|
11/3/2017 10:26 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by IT service is split to a separate thread with the subject Picture tree of clients . Best regards |
Follow us on