Industry Online Support
Technical Forum
8/21/2013 8:28 PM | |
Joined: 9/27/2006 Last visit: 5/28/2024 Posts: 12257 Rating: (2668)
|
Hello Andy; What software do you use to program the OP17, ProTool? Is ProTool integrated ith Step 7, which allows direct import of the Step 7 tags into the HMI, or has this been done by hand? SIMATIC HMI ProTool How to configure text-based units In any case, start by opening the TAGs directory in the poject window (see the attachment below) to verify that the correct DB is addressed with the faulty tags. Hope this helps, Daniel Chartier |
Follow us on