8/1/2023 7:16 PM | |
Joined: 12/18/2014 Last visit: 8/13/2024 Posts: 33553 Rating:
|
You can adjust the parameters of the PI controller for this. |
8/3/2023 5:03 PM | |
Joined: 5/2/2023 Last visit: 8/10/2024 Posts: 8 Rating:
|
Hi, i'm a bit lost here. I tried but fail to make it work. Maybe my starting point is not usable since i do not read an 0-10v. I use flow meter, connected to a high speed Input port. This Input port is then converted in liters per hour ( B045), then displayed on the Logo and a HMI I have build some coding to manually change the flow speed . Now I'm looking to have the speed automated to lets say 1800 LPH and here i'm stuck. Please see the pic and the attached file. AttachmentSPEED CONTROL.zip (425 Downloads) |
Follow us on