3/7/2012 2:30 PM | |
Joined: 11/28/2011 Last visit: 4/20/2023 Posts: 53 Rating:
|
I would like use some siemens aplication - program for the speed monitoring and maybe limitation . We have machine and this must run in 3 diferent speed modes if we change operating mode or for the safety reason. 3km/h , 7km/h, 250km/h , somethink like. I hope that exist some FB or some safety blocks in Safety area , we use 1Count module up to 500kHz for the reading value. I found also some manual from siemens can I use this??? Thank you very much for any idea or help !!!!!! B.R M. Chyska AttachmentPDF1A70_print.pdf (59 Downloads) |
3/15/2012 8:31 AM | |
Joined: 10/10/2005 Last visit: 3/16/2023 Posts: 1909 Rating:
|
Hello, this is a description for the special application (standstill, direction methode, ...) which do you can use. Regarding to speed monitoring please find the application in the internet (link): http://support.automation.siemens.com/WW/view/de/51445385 With best regards |
Follow us on