6/30/2017 2:38 PM | |
Posts: 1529 Rating: (203) |
Did you tune the drive? The speed feedback should closely follow the reference. Yours is awful. |
6/30/2017 2:57 PM | |
Posts: 16 Rating: (0) |
yes. we optimized the drives. Actually it the first drive in the polyester draw line. There might be a pulling effect from the other drives after this one which cause it to deviate from reference. But when the line stops, this drive moves a little but the reference at the RFG is zero. This confusing. i have attached the Drive backup. AttachmentPrefeed_290617.zip (214 Downloads) |
Last edited by: OMerfayyazzz at: 6/30/2017 2:59:41 PMLast edited by: OMerfayyazzz at: 6/30/2017 3:13:58 PM |
|
7/1/2017 3:02 AM | |
Posts: 1529 Rating: (203) |
Do you have a tension/dancer position loop or some other correction outer loop? That will be after the RFG. |
Follow us on