11/27/2006 1:31 PM | |
Posts: 3149 Rating: (171)
|
Hi, NEVER start WinCC-RT on your Engineering station...please always use OS-Simulation => http://support.automation.siemens.com/WW/view/en/22030431 http://support.automation.siemens.com/WW/view/en/17498343 nemo |
11/30/2006 8:02 AM | |
Posts: 122 Rating: (4) |
thanks very much |
12/11/2006 11:18 AM | |
Posts: 122 Rating: (4) |
dear April: you are right,i didn't find the "start simulation"just because my WINCC is in the lower version. |
12/12/2006 12:57 PM | |
Joined: 9/13/2005 Last visit: 11/18/2019 Posts: 86 Rating: (10)
|
Hello peters, you should also consider this FAQ http://support.automation.siemens.com/WW/view/de/24285103 Unfortunatelly this FAQ is only available in German at the moment, but I am sure the translated version will be published soon. FAQ 24285103describes the steps which are necessary to fix the project when you accidentally started OS Runtime (Serverproject) on the ES instead of using OS-Simulation |
Best Regards - Mit freundlichem Gruß - yoroshiku onegaisimasu - Sincères salutations |
|
12/15/2006 5:12 AM | |
Posts: 122 Rating: (4) |
thanks very much! |
Follow us on