11/5/2024 12:30 PM | |
Joined: 1/13/2021 Last visit: 2/23/2025 Posts: 1 Rating:
|
Hi everyone I have problem with connected to SQLite connection string is "Driver=SQLite3;Database=media/simatic/X61/HMI_RT_3_TLG243_20241105_092615.db3;trusted_connection=yes;" and Query is "SELECT*FROM LoggedProcessValue;" error apear is error state LoggedProcessValue(1) error Message HY00 kindly look at attached file for js ------------------------------------------------------------------------------------------ AttachmentNew Text Document (4).txt (53 Downloads) |
Last edited by: Moderator_Lan at: 11/05/2024 12:33:26New subject after splitting |
|
11/5/2024 1:00 PM | |
Joined: 7/11/2024 Last visit: 3/14/2025 Posts: 150 Rating:
|
Hi Ali, Which version of Unified are you using? which image version do you have in the panel? Have you tried deleting the DCF file? It might be incosistent Update the configuration file of the WinCC project (delete DCF) Good luck! |
If this post has been useful, don't forget to rate it!😊 |
|
Follow us on