6/17/2024 5:08 AM | |||
Joined: 3/11/2019 Last visit: 7/3/2024 Posts: 1504 Rating:
|
Hi, yes, the 6ES7 414-5HM06-0AB0 is a V6 variant. CPU414-5H PN/DP, 4MB F. S7-400H/F/FH
regards sancruz |
||
Feedback appreciated, please rate |
|||
6/17/2024 7:25 AM | |||
Joined: 6/14/2024 Last visit: 6/22/2024 Posts: 3 Rating:
|
Yes, the 6ES7 414-5HM06-0AB0 is definitely a V6 variant, but I'm not sure about the "S7-400 PN/DP V6" part. As far I know: S7-400 PN-CPU V6 (PN/DP) - standard CPUs - for example 412-2 PN, 414-3 PN/DP S7-400 H-CPU V6 - high-availabilty CPUs - for example - 414-5H, 414-5H PN/DP SSA affected products table: "SIMATIC S7-400 PN/DP V6 and below CPU family (incl. SIPLUS variants): All versions" Doesn't this mean that the affected products are the standard CPUs? I think that if SSA-731239 referred to the 414-5H PN/DP it would be for example SIMATIC S7-400 H V6 CPU family? or I am wrong? |
||
This contribution was helpful to
1 thankful Users |
6/21/2024 5:43 AM | |
Joined: 3/11/2019 Last visit: 7/3/2024 Posts: 1504 Rating:
|
HI, thank you for the update and feedback! I got this wrong! regards sancruz |
Feedback appreciated, please rate |
|
Follow us on