Industry Online Support
Technical Forum
5/6/2013 11:05 AM | |
Joined: 8/31/2010 Last visit: 5/10/2024 Posts: 1509 Rating: (222) |
Hello Jorsal, Am not sure if this update can help you - Updates for STEP 7 V12 and WinCC V12 All what you can do is, first find out the occurence (based on your working experience with TIA Portal) on when the software crashes. Once you are able to locate it then try to perform the operation which you desire using some work around. In this way I have minimized the crashes by taking diversions then and there I know this is not the right way to handle it. But you can also contact the Industry Online Support via Support Requestso that they can support you. If its a known case, they can suggest suitable; whereas if it is not known, then it can berectified in future SPs / Updates.
|
Like it? Rate it! |
|
This contribution was helpful to2 thankful Users |
Follow us on