1/12/2015 1:12 AM | |
Joined: 2/3/2011 Last visit: 5/30/2024 Posts: 6 Rating:
|
hi In accordance with Attachment diagnostic buffer my standby cpu of plc 414-4h for sync module error go to stop mode. IFM1F AND REDDUNDANCY LED IN BOTH CPU IS ON AND EXTR LED RELATED TO STANDBY CPU ALSO WELL AS IS ON. I REPLACED BOTH SYNC MODULE FOR IF1 IN MASTER AND STANDBY CPU AND ALSO FO PATCH CABLE FOR TOP SYNC MODULE BUT ERROR LED NOT CLEAR.PLEASE HELP ME WHATS PROBLEM AND What should I do for troubleshooting Attachmentdiagnostic buffer.zip (184 Downloads) |
1/13/2015 2:58 PM | |
Joined: 1/28/2009 Last visit: 6/26/2024 Posts: 6841 Rating:
|
If you are sure of accessories like fiber optic cable and SYNC Module,In such case I test the CPU individually.When a CPU intermittently report that an intact SYNC Module is not available and then available several times, perhaps some thing is wrong with mechanical or electronics parts inside CPU that keep and detect the existence of SYNC Module.In this case, I suggest consulting with people HERE (Support Request).
|
Follow us on