1/20/2023 4:46 PM | |
Joined: 6/27/2010 Last visit: 6/5/2024 Posts: 2 Rating: (0) |
Hello, I have two SFC Types : First SFC Types have three control strategies : START,STOP,OFF Second SFC Types have the control strategies : START,STOP,OFF It's possible when I start first SFC Types, sequence START , in Step 01 , to start automatically sequence START for second SFC Types? In first SFC Types ,need to have feedback if sequence START for second SFC Types is ON. The same logic need to apply for Sequences STOP and OFF . How can do this, in the best and safe way? ------------------------------------------------------------------------------------------ |
Last edited by: lazarvlad at: 01/20/2023 20:32:22Last edited by: Jen_Moderator at: 01/23/2023 09:52:46New subject after splitting |
|
Follow us on