7/6/2015 10:01 AM | |
Posts: 1 Rating: (0) |
Dear Siemens , I was installed starter 4.3 in my pc.installation was completed sucessfully. Open starter software without any error,but when create new project then given name of project starter software was hang & not work. My laptop configuration windows Xp sp3 & 120 GB harddisk & 2 GB Ram as per starter software requiement. Reistall starter software 4.3 ,but same problem. so what will i do.............
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/6/2015 4:04:55 PMNew subject after splitting |
|
7/9/2015 9:49 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating: (797)
|
Hello AutoGen, do you need to use STARTER 4.3 since there is already STARTER 4.4 released: https://support.industry.siemens.com/cs/de/de/view/26233208 If not, please open a service request since the would need to check whether there is a general SW issue given you hardware and software setup. http://www.siemens.com/automation/support-request Thaks! |
With best regards, |
|
Follow us on