10/31/2019 2:00 PM | |
Joined: 5/16/2017 Last visit: 4/5/2024 Posts: 10 Rating: (0) |
Hello Navnag, I hope that you see my post somehow, because I have similiar problem that you had. I have Starter 5.3 and when I try to open a project of one of our machines, there is a message window: Missing software packages. The following objects in this project cannot be processed as the appropriate software packages have not been installed. Object: S110_CU305_PN, Object type: SINAMICS S110 CU305 PN V4.4, Software package V4.4. Moreover when I try to connect to this unit in order to upload the project from it, the unit is on found nodes list, but it's uncaccessible, which is caused by this missing software package I guess. I installed the SSP SINAMICS V4.4 SP3 and when I look at the Installed Devices in Starter there is on list device: SINAMICS S110, CU305 PN, V4.4.3 (version internal V4.40.44.00), SSP SINAMICS V4.4 SP3, release version V04.40.44.00_11.26.00.00. So what could be the problem? Did you manage to resolve this problem? Thanks for any tips. Lucas. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/04/2019 09:04:59New subject after splitting |
|
11/6/2019 8:38 AM | |
Joined: 5/12/2006 Last visit: 4/30/2024 Posts: 22243 Rating: (2980) |
hello, the ssp is in the starter install data! VOL2 of the downloads of starter setup Regards Christoph |
Follow us on