7/5/2017 12:23 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hell, can you attach the file here for analyze? Regards Christoph |
7/6/2017 6:57 AM | |
Posts: 8 Rating: (0) |
Hi ChristophD, Thanks for your reply, the file size is larger than the forum maximum limit 3MB, so I uploaded it onto google drive :link total 4.14MB MD5: 9bbe36d0e9df95ecfc43a69bac1d52af BR/Li |
3/29/2018 3:16 PM | |
Joined: 3/20/2017 Last visit: 8/15/2023 Posts: 5 Rating: (0) |
can someone need a solution. I had a too long way to file. |
3/29/2018 3:32 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
I don´t know, maybe your Trace file is very big? |
4/11/2018 8:14 AM | |
Posts: 15 Rating: (1) |
The file name should be the following format: kl-install-yyyy-mm-dd-hh-mm-ss.log kl-setup-yyyy-mm-dd-hh-mm-ss.log
|
Follow us on