7/24/2019 8:31 PM | |
Posts: 3 Rating: (0) |
Am also facing same sort of problem. Am trying to replace cu320 with a cu320-2dp module. Am having starter which worked fine with cu320. But after replacement starter is not detecting cu320-2dp in accessible nodes. if i roll back to cu320 everything works normal. i checked set pg/pc interface profibus.( bus in diagnostics it says not node found on the network) access point as -device SSPs are installed ( including the version its matching) My total system is 1.S7 300 plc On this PLC profibus n/w it got a. two position encoders. b. one s120 drive with cu320 2. for cu320 one incremental encoder for speed control with SMC Card. Any help Thank You. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/25/2019 07:30:44New subject after splitting |
|
7/25/2019 5:58 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating: (3003) |
Hi, how is the LED Status of CU320-2 DP? Christoph |
Follow us on