6/25/2020 2:50 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
Did you configure the same telegrams in TIA Portal as in STARTER? |
|
|
6/29/2020 12:35 PM | |
Posts: 8 Rating: (0) |
I add a picture how do I send the words to/from TIA! |
6/29/2020 12:40 PM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981) |
Hi, you send only data to the CU (Slot1) of the slave. No Slots for Infeed or Motormodules defined. regards |
7/2/2020 2:29 PM | |
Posts: 8 Rating: (0) |
Dear All, I attached the pictures of SCOUT and TIA Portal with the profiibus communication problem that I am faceing. Can someone help me to understand what's wrong? [snip] here there is 6 pictures: 1. telegram structure in SCOUT with below the alarms I get after RAM to ROM transfer 2. the I/O modules configurated on Siemens TIA Portal 3-5 function for I/O drive communication telegram 6 "No master" message when I try to see online the telegram values on Scout Looking forward to your answer! AttachmentItems Shared on 7-2-2020.zip (235 Downloads) |
Last edited by: Jen_Moderator at: 07/03/2020 08:03:02Removed link and added file as an attachment. |
|
7/2/2020 6:05 PM | |
Posts: 8 Rating: (0) |
I did as you told me but there is still something going on ......please look on the picture I took ! |
7/3/2020 12:00 AM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
No axis seperator between Tel370 and Tel102 (of servo_3) ? (I don't know, if it is required) |
|
|
Follow us on