Industry Online Support
Technical Forum
6/27/2011 7:48 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Best regards, Hristo Mihalev |
6/27/2011 12:31 PM | |
Joined: 12/2/2010 Last visit: 4/2/2024 Posts: 61 Rating: (0) |
Hi, Please provide some sample program for getting channelstatus of each module.(Third party SCADA). |
Regards \ Sankar |
|
6/27/2011 12:53 PM | |
Joined: 8/20/2009 Last visit: 5/21/2024 Posts: 80 Rating: (5) |
Dear Sankar, There are some blocks available in the library for this purpose. Also uwill needto use some system blocks. U can connect Quality output tothe addressesor useTx of send/recieve blockfor transfer to the third party SCADA or DCS. For the reference I have attached a snapshots of the block use and interconnection. Regards, Vishal Parmar --------------------- Rate it if useful. AttachmentAI-DI Diagnose.zip (121 Downloads) |
Vishme. |
|
6/27/2011 12:59 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
In case of third part SCADA you should manually generate all the data using SFC51 and OB82 eventually. Like in http://support.automation.siemens.com/WW/view/en/19215174 http://support.automation.siemens.com/WW/view/en/19952036 Best regards, Hristo Mihalev |
Follow us on