8/2/2017 5:10 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating: (2678)
|
Hello bhipune; The following Application examples shows 2 ways of establishing and monitoring on a Siemens HMI the status of an ET 200S station over Profinet, one through data recor search, one through FB 126 "PNIODiag". PROFINET IO – Diagnostics Processing in the User Program Look at section 8.2 and 8.3 to see the available diagnostic screens on the MP 300 used in the example. Here is a link to download FB 126 if you decide to go that route: Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO (STEP 7 V5.x) Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/2/2017 5:12:43 PM |
|
This contribution was helpful to2 thankful Users |
8/4/2017 9:40 AM | |
Joined: 4/28/2015 Last visit: 7/10/2024 Posts: 42 Rating: (1) |
hi,sir Daniel application work using fb126. thanks for help. |
This contribution was helpful to1 thankful Users |
Follow us on