9/5/2015 3:40 PM | |
Posts: 2 Rating:
|
Hi all, just wondering since you are using STEP 5 on a XP guest in VMware, how do you connect to a PLC? Are you connected via Ethernet and a monkey tail on the PLC, linking Ethernet card to PG port on the CPU? This works fine on our phycical XP PC's, but not in the virtual enviroment. On the guests and phycical machines I have STEP5 7.23 HF1 and Simatic Net 2008+SP2. Simatic Net 2008 SP2 (v.7.1) does not support VMware, Simatic Net 8.2 does support VM but not Windows XP, so its not possible to match. The problem is, on a XP guest im not able to select the network card in Simatic Net configuration, proberly since the non VMware support. Running STEP5 issen't much fun, if you can't get online :) Best regards Lars Denmark. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/7/2015 3:34:59 PMNew subject after splitting |
|
9/8/2015 4:33 PM | |
Posts: 8946 Rating:
|
Try to use an USB - TTY adaptor! |
9/9/2015 3:39 PM | |
Joined: 11/21/2007 Last visit: 3/31/2025 Posts: 2326 Rating:
|
Hello Jürgen Can you recommend any Model ? Thanks Navnag |
There is no such thing as the last bug in a program |
|
9/9/2015 4:10 PM | |
Posts: 8946 Rating:
|
There are a lot of them, one example: |
This contribution was helpful to
1 thankful Users |
10/22/2015 8:23 AM | |
Posts: 2 Rating:
|
Hi, and thank you for your great suggestion. This will most likely do fine on a laptop, but what Im trying is to get at up and running is in a server enviroment with multible VMware hosts, and reach multible STEP5 PLCs over our ethernet. My bad, I haven't replied erleyer, I thought I got an email when there were new posts in a thread :) I'll better look into settings and see if its possible. Best regards Lars |
10/22/2015 9:39 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Thank you for the feedback Lars! But that options it is not useful in some cases. Is it? many emails... Best regards, Hristo Mihalev |
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on