9/29/2015 10:57 AM | |
Posts: 93 Rating:
|
Thanks William for response. I have windows XP and using STEP5 /ST Version 7.14. |
9/29/2015 6:12 PM | |
Posts: 8946 Rating:
|
You may do the update Step5 V 7.23, some bugfixes for 135U was done there. Also you may read this thread: https://support.industry.siemens.com/tf/ww/en/posts/94003/ OK, back to Topic: - First connect the PLC with correct cable to correct TTY - port of PG. - Start Step5 - Push F4 button to go to project setting screen - Push F3 button to Switch over to ONLINE mode. - Press ENTER or INSERT to accept and go back to main screen or - Push ESC to go back to main screen - Push Shift+F6 and select the block that you like to monitoring online. - Push Shift+F8 to control variables - Push Shift+F5 to control output |
This contribution was helpful to
6 thankful Users |
9/30/2015 10:35 AM | |
Posts: 8946 Rating:
|
Please read my post more careful. Shift+F8 is valid im Main Screen, not in the Block Screen. Find attached some screenshots: 1_MainScreen.jpg = here the "Status" shortcuts are active. 2_handlinginfo.jpg = use the help function to learn more about S5 user interface 3_projectsetting.jpg = the path to go to the Online - selection screen 4_select_online_F3.jpg = here you select between ONLINE and OFFLINE mode. Consider also: Sometimes it is necessary to Switch OFF the NUMLOCK and using the numeric pad. Attachments5monitor.zip (521 Downloads) |
Last edited by: IBN-Service at: 9/30/2015 10:38:17 AM |
|
Follow us on