1/14/2017 11:15 AM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: Which version of STEP 5 is compatible with which MS Windows operating system? |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to2 thankful Users |
1/14/2017 11:27 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello, pay attention you need also the cable to connect PC to S5 Using the cable 6ES5 734-1BD20 for connect PLC to PC - Entries ... or http://www.cdelektronik.de/products/S5_PG-USB/s5_pg-usb.html |
This contribution was helpful to2 thankful Users |
1/18/2017 4:50 AM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
Dear Best is this u used Windows XP based system with built in serial port option. |
Muhammad Munir |
|
9/4/2019 1:36 AM | |
Joined: 5/20/2009 Last visit: 6/25/2024 Posts: 3 Rating: (0) |
You can create a VM with window XP (or other OS). I recommend to use a PG95 SW if you do not have other. JAFAM |
Follow us on