Industry Online Support
Technical Forum
1/4/2012 1:35 PM | |
Joined: 4/24/2006 Last visit: 12/20/2024 Posts: 8786 Rating: (1172) |
Hello QUAD_Mark, Perhaps this link might help: Which settings and procedures are to be observed with regard to InstallShield when installing STEP 7? Best regards, Wizard |
1/4/2012 1:39 PM | |
Joined: 3/21/2006 Last visit: 1/3/2025 Posts: 10234 Rating: (1181) |
Hello, Take a look at TIA Portal (V10.5 or V11) DCOM Installation error Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
1/4/2012 5:35 PM | |
Posts: 2 Rating: (0) |
Solved my problem by using the instructions listed on this forum below, basicly DCOM was not running on my laptop...and could not be started... after re-installing MSDTC and registering the dll file "mtxoci.dll" then resetting the default properties for Distributed COMmy computer to Default Authenication = Connect and the Impersonation Level = Identify Reboot... and now the service is running and the installer is now installing SP2 here is the link to the information that solved it for me. Jackuars solution Thank you for the help! Mark |
This contribution was helpful to1 thankful Users |
Follow us on