6/2/2021 11:33 PM | |
Joined: 3/4/2006 Last visit: 11/15/2024 Posts: 73 Rating: (3) |
I have successfully rolled back to Step 7 prof 2017. Not sure if we will ever learn why this was released. |
6/7/2021 6:01 AM | |
Joined: 3/4/2006 Last visit: 11/15/2024 Posts: 73 Rating: (3) |
No doubt you've seen this link STEP 7 V5.7 / S7-GRAPH V5.7 / S7-SCL V5.7 / S7-PDIAG V5.7 / STEP 7 Professional 2021 Trial Download Interestingly, the SHA256 hash for the Professional 2021 ISO matches the file I downloaded. |
6/8/2021 8:15 PM | |
Joined: 11/3/2020 Last visit: 8/15/2024 Posts: 1 Rating: (0) |
i have the exact same problem. is the only way to clear the fould to instal a older version of the simatic manger? |
6/22/2021 5:50 PM | |
Posts: 4 Rating: (1) |
I have just installed my SUS software detailed above and the same has happened to me. I have repeatedly uninstalled and reinstalled Wincc Flexible and Starter (SIMOTION). The issue remains. I have put a support request into siemens, If I get a solution I will update this thread. Thanks to you all for your comments. Siemens Response: Please see the link below as promised. After installing STEP 7 V5.7, why do you get a message about missing options packages when starting STEP 7? |
Last edited by: Protologic at: 06/23/2021 10:49:43Last edited by: Protologic at: 06/23/2021 16:54:59 |
|
This contribution was helpful to2 thankful Users |
Follow us on