10/14/2008 9:51 AM | |
Joined: 9/27/2006 Last visit: 9/24/2023 Posts: 12153 Rating:
|
Hello @Js; Step 7 allows for multilanguage setups, as you can ssee in the following extract: From the programming with Step 7 V. 5.4 manual: 6.8 Managing Multilingual Texts STEP 7 offers the possibility of exporting text that has been created in a project in one language, having it translated, re-importing it, and displaying it in the translated language.The following text types can be managed in more than one language: • Titles and comments - Block titles and block comments - Network titles and network comments - Line comments from STL programs - Comments from symbol tables, variable declaration tables, user-defined data types, and data blocks - Comments, state names, and transition names in HiGraph programs - Extensions of step names and step comments in S7-Graph programs • Display texts - Message texts generated by STEP 7, S7-Graph, S7-HiGraph, S7-PDIAG or ProTool - System text libraries - User-specific text libraries - Operator-relevant texts - User texts Also here, you will find a collection of FAQs on Multilanguage setups in Simatic manager: http://support.automation.siemens.com/WW/view/en/22523230
|
Last edited by: dchartier at: 10/14/2008 9:52 AM |
|
Follow us on