10/20/2007 9:27 PM | |
Joined: 1/7/2006 Last visit: 2/16/2023 Posts: 2705 Rating:
|
Hi, The ST7 and TD7 software are coming together and have to be ordered. There are some handbooks on internet that could explain a lot, the SINAUT system is for telemetry and is a system, not a manner to built it up by your own. SINAUT ST7 System Manual, Volume 1: System and Hardware SINAUT ST7 System Manual, Volume 2: Software It is possible to couple one network to the TIM 3V IE, serial or ethernet, there must be at least one master in the network. You can couple Analog and ISDN Diallines, standlines, GPRS, GSM, ADSL, IE, Radio (serial and Ethernet). |
Last edited by: Late at: 21.10.2007 21:45Link corrected I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on