9/9/2023 10:07 PM | |
Joined: 4/23/2021 Last visit: 7/10/2024 Posts: 1 Rating: (0) |
During installation S7 V5.6 in the last movement process stop and waiting for simplify project. ZEN01_10_STEP7_COM_SFB. Installation not complete ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/11/2023 11:31:11New subject after splitting |
|
9/11/2023 12:19 PM | |
Joined: 5/6/2022 Last visit: 7/30/2024 Posts: 436 Rating: (84) |
Hi manojkm, My recommendation is that if you are installing from the DVD, try to install from the downloadable one. I share it with you below: STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial Download On the other hand, we recommend that you check that you are complying with the following points: - Operating System that is compatible with the software. You can check it from the 'Compatibility Tool' - That you do not have any firewall/antivirus activated. - That you are working as an admin. Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on