8/10/2015 12:18 PM | |
Joined: 5/12/2006 Last visit: 10/11/2024 Posts: 22410 Rating: (3017) |
Hello, in the FAQ If you have any other Packages installed like WinCC or PLSIM or Safety then uninstall this packages. After the uninstall you should delete old logfiles manually and then start the new installation.
Christoph |
8/10/2015 3:23 PM | |
Posts: 8 Rating: (0) |
OK, here I attach the complete logfile. Yes, I tried once disabling the AntiVirus and I still got the 3 errors. There is not any Siemens folder in Program Files (x86) and I don´t find in the Registry HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Siemens\Automation\TIAP13 Besides this, I don´t know if it is relevant, but before starting the installation the folder C:\ProgramData\Siemens\Automation\Logfiles\Setup was empty. Thank you for your help! AttachmentSIA_STEP7_PRO_V13@15-08-10_15-07-14_AFTERREBOOT.txt (375 Downloads) |
8/10/2015 3:29 PM | |
Posts: 8 Rating: (0) |
Here I also attach the sumary. Thanks!
AttachmentSIA_STEP7_PRO_V13@15-08-10_15-07-14_AFTERREBOOT_summary.txt (371 Downloads) |
8/10/2015 4:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
|
Follow us on