3/31/2010 10:31 AM | |
Joined: 10/7/2005 Last visit: 7/25/2024 Posts: 3011 Rating: (1053)
|
Hello xblackx don't worry too much about this, you probably copieda"pj.ini" that is part of a step 5 project from another PC (which had the S5 project stored ontheE: drive). The pj.ini is a simple text file that you (or others) create via Step 5 to "memorise" your S5 project setting for easy retrieval the next time you want to work on it (e.g.directory of your S5 files, S5 file name,Symbol file name,header/footer setup etc.). Simply make a new "pj.ini"which has the correct settings for your S5 project and your problems will go away (have a look at chapter 3.2.1 of THIS Step 5 manualfor your versionwhich has more on this). I hope this helps |
Cheers |
|
3/31/2010 11:05 AM | |
Posts: 5 Rating: (0) |
hello fritz Thank you for your help first. e: cd rom,if any cd in the cdrom drive,This error does not happen. don't update V6.68 (2.message) best regards |
Follow us on