1/8/2021 6:42 PM | |
Posts: 198 Rating: (17) |
Hello, I need help finding step7 5.2 sp1 for NCM it self. Website says : there is a separate download but cant find it. entry id : 16540054 TheService Pack 1(SP1) forSTEP 7 V5.2is now available on CD ROM and can be ordered at a nominal fee from your SIMATIC contact at your local Siemens office. It is also available for free downloading from the Internet (entry ID16540057. A separate download will be provided for NCM S7 for PROFIBUS and Industrial Ethernet V5.2). Clients with a valid Software Update Service agreement for STEP 7 or STEP 7 Professional will receive the corresponding CD ROMs automatically. Probabily this was old link : https://support.industry.siemens.com/tf//WW/en/posts/hw-config-step7-v5-2-sp1/26189?page=0&pageSize=10 http://support.automation.siemens.com/WW/view/en/19027119 however it seems deleted. |
1/8/2021 7:20 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33161 Rating: (4095) |
Start a Support Request ... |
This contribution was helpful to1 thankful Users |
Follow us on