1/22/2010 8:24 PM | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
OLD_tom wrote in a private message:
Dear Old Tom, 1. Step7 Lite is not compatabile with Windows 7. Please have a look on the following link: Which version of STEP 7 Lite is compatible with which version of MS Windows operating system and optional software package and which version of the Internet Explorer is required? 2. I can not guess which version you have of Step7 Lite. In any case, as you know that Step7 Lite is a free of charge and it is available for downloading from the internet. Here's the latest version of Step7 Lite link: STEP 7 Lite V3.0 incl. SP4 Available for Downloading 3. As it's a freeware, I think you should know what's the differences between Step7 Lite, Step7 and Step7 professional.Here's bellow in the following table the differences.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: Ayman Elotaify at: 1/25/2010 10:54 AMAyman Elotaify |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to1 thankful Users |
6/28/2014 4:11 PM | |
Posts: 2 Rating: (0) |
Hi Ayman Will there eventually be a version of Step 7 lite that will be compatible with MS Windows 7? Regards Balleka |
11/26/2015 5:39 PM | |
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685)
|
Hello Arturas; Interesting... specially since this appears to be a v. 2.0 of Step 7 Lite, not even the freely downloadable version found on Siemens' site (v. 3.0): https://support.industry.siemens.com/cs/ww/en/view/22764848 My own attempts at using Step 7 Lite on any platform above XP SP1 were ineffectual (but I am not a Windows guru, so that was to be expected). In any case, Step 7 Lite has always been a very limiting package, without communications or Fieldbus connections; it was useful for very basic training purposes. Regards, Daniel; Chartier |
11/29/2015 12:31 PM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839)
|
Hello, Nobody told that it's compatible with MS Windows 7! Did you checked this link -which already published in the first post here-: Which version of STEP 7 Lite is compatible with which version of MS Windows operating system and optional software package and which version of the Internet Explorer is required? |
Ayman Elotaify |
|
12/8/2015 7:55 AM | |
Joined: 1/27/2009 Last visit: 9/17/2024 Posts: 172 Rating: (8) |
Hello Daniel Yes, it is limited, but i have 1 project made by Step 7 Lite, and as far as i know Step 7 cannot open Lite project. Also, i am not familier with Lite but seems like V2.0 was paid version? as i have got CD and a yellow floppy with a license. BR @rturas |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
12/8/2015 7:57 AM | |
Joined: 1/27/2009 Last visit: 9/17/2024 Posts: 172 Rating: (8) |
Hello Ayman, I've tried to install V3 but got compatibility message and installation cancels itself. BR @rturas |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
Follow us on