12/1/2023 2:54 PM | |
Joined: 7/19/2022 Last visit: 6/28/2024 Posts: 373 Rating: (61) |
Hello Siemens_User_CWBox, You would need to install WinCC Flexible because you have a HMI inserted. Also, I would update all the HSPs. You can download the HSPs from: STEP 7 V5.x Hardware Support Packages (HSPs - as at 10/2023) for installing hardware updates in the Hardware Configuration Here you have more information in this FAQ: After installing STEP 7 V5.7, why do you get a message about missing options packages when starting STEP 7? |
If this Information really helps, you could use the Rate function |
|
Follow us on