Industry Online Support
Technical Forum
3/16/2011 10:34 AM | |
Joined: 10/7/2005 Last visit: 5/21/2024 Posts: 3005 Rating: (1048)
|
Hello Drip44 your blockmove related code looks ok and won't be the cause of your "shifting" problem. I understand thatyou are actually using the data type "STRING" correct? If so, the "shifting" comes from the fact that the first Byte of a String contains a value that indicates the maximum stirng lenght and the second byte contains avalue for the actual string lenght. TheS7 inbuilt help has more on this and I hope this helps. |
Cheers |
|
Follow us on