11/30/2012 10:18 PM | |
Joined: 7/7/2010 Last visit: 10/16/2024 Posts: 15319 Rating: (2432)
|
Add a new tag after Static_1. You will then see the offset. You can also create 11 individual DWord tags and the offsets for each will appear. The offsets from _within_ the array will not be shown. If you create a structure called Static_1, then create 11 DWords, named Static_1_0, Static_1_1, ... , Static_1_10, and all offsets would then appear if I recall correctly. Structures and individual tags give you offsets. Arrays do not. Perhaps in V12 that will be changed? Maybe you can submit a Support Requestasking for a work-around? |
science guy |
|
This contribution was helpful to1 thankful Users |
11/30/2012 10:45 PM | |
Joined: 1/17/2006 Last visit: 10/14/2024 Posts: 553 Rating: (29) |
huggy_d1, Thank you for your help. I've already sent this issue to Siemens support as you advised me. Best regards, Berg |
"Educate the children and it won't be necessary to punish the men." |
|
This contribution was helpful to1 thankful Users |
Follow us on