10/20/2006 2:48 PM | |
Joined: 10/10/2005 Last visit: 7/18/2024 Posts: 1917 Rating: (136) |
Hello, regarding to your inquiry we would like to inform you. But we can not reproduce your described question or problem. Please see our attached example program with your program code in FC1and the DB20 we have declared with the variable of type of ARRAY [1..20] OF DWORD. If we load the complete program code (FC1 is called in OB1) in the CPU, the lowest bit will be set in DBD0 (Address 0.0, Variable [1]). With best regards Cicero AttachmentPtest2.zip (541 Downloads) |
10/20/2006 4:37 PM | |
Posts: 3 Rating: (0) |
I see my problem. I had my Datablock defined as five words but I was using DBD which, I now realize, implies a Double Word. Thank-you for your help. |
Follow us on