7/13/2014 7:17 PM | |
Posts: 8946 Rating: (999) |
Yes, theydo also. Same thing S and R and Jumps.... |
7/13/2014 7:25 PM | |
Posts: 8946 Rating: (999) |
? I dont think so. |
7/13/2014 9:51 PM | |
Posts: 69 Rating: (0) |
Could you clarifie a bit more ?
|
7/13/2014 10:01 PM | |
Posts: 69 Rating: (0) |
I have written a simple program in STL the purpose of it is to exercise my new limited skills. The program controls a ATS panel and a generator to turn on and off, i have attached the file and would be thanksfulif you could give me your thoughts and adivce. Thanks in advance
AttachmentOB1.pdf (136 Downloads) |
7/14/2014 9:15 AM | |
Posts: 8946 Rating: (999) |
PLEASE Use a new network for any allocation. |
7/14/2014 9:23 PM | |
Posts: 5225 Rating: (1192) |
Hi Mishal11. Please find attached a sample code piece that represent the code structure I think you aimed for originally. The image was created in Step7 for TIA.. you will not have the "%" signs in your version of Step7. The LAD and converted STL version are shown. What I saw in my mind for the coding looks different from how the code actually turned out. My comments on execution speed is not true for the reasons I had in mind for. You will see in the STL converted code some NOP commands. These are placeholders for the full functionality of the timer as seen in LAD. You can leave these no-operations out and the code will still execute correctly - BUT the coding will then not be able to convert back to LAD. NOP commands does take some of the scan time to scan over, but it is a very small period. I think you will find it interesting how the "(" and ")" was used in the attached example. w |
7/14/2014 9:27 PM | |
Posts: 5225 Rating: (1192) |
- - - about your code... Purely out of an academical point of view, you could have done the following structure.. [code]// Global time value L S5T#4s // Check if I0.0 is held for a while A I0.0 SD T0 // Check if I0.1 is held for a while A I0.0 SD T1 //..will use 4 seconds again because Acumulator did not change // Switch Q0.0 if either timer is ON, but not if both A T0 X T1 //..simple bit XOR, not directly available in LAD = Q0.0 [/code] Note the time value is loaded once but re-used. That is possible because the accumulator is not updated with another value and the coding is in one network. In the following code the accumulator is again re-used: [code] L #value //smaller than 5 L 5 <I = #M1 //equal to 5 ==I // accumulators still in place = #M2 //bigger or equal to 10 TAK // swap accumulators.. as if "L #value" L 10 >=I = #M3 // value is between 6 and 9 AN #M1 AN #M2 AN #M3 = #M4 [/code] ------- IBN-Service is giving you deep rooted advice - I am going to add to it. STL is a very powerful tool. You can create very effective coding with it. There is however a danger too. You must be very aware of how the code will be handled and executed; it is very easy to make a slip-up. As an example, if you split the coding to more networks, there In this days you should consider also how much understandable and readable your code is. When using multiple netwroks, you force yourself to (hopefully) document smaller portions of your code. It does not help you designing very clever code that you can not even follow yourself in 3 months' time. If you have to make an analasys of such code just to understand what it does.. your clever code waisted your time when a breakdown comes. The rules change however when you design code for interrupts.. there your code should be as effective as ever. I very much liked using STL coding. Using SCL instead has however other advantages. There are web pages where you could get coding for solving some problem that is easily converted to SCL. Having said that, I'd rather use LAD or STL when coding timers. I hope you find these thoughts helpful. w |
Last edited by: William B. at: 7/15/2014 12:04 PMwording strike through Last edited by: William B. at: 7/14/2014 9:30 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on