3/17/2015 11:13 AM | |
Posts: 19 Rating:
|
Hello, Can someone help me in converting STL program to LAD program? I have a program with Function Blocks written in STL which will support S7-300 & S7-400 series PLC's. But same program blocks are not supported in S7-1200 series PLC's because 1200 PLC is not supporting STL language program blocks using TIA Portal V11. Is there any conversion tool available in Siemens for easy conversion? Thanks in advance.
---------------------------------------------------------------------------------------------------- |
Last edited by: Sai442 at: 3/17/2015 11:14:17 AMLast edited by: Min_Moderator at: 3/17/2015 1:53:02 PMNew subject after splitting |
|
3/24/2015 6:38 AM | |
Posts: 19 Rating:
|
Hello, Can someone help me in converting above logic to LAD? This is very much important for me. Please help. Thanks in Advance.
Saidulu |
3/24/2015 6:46 AM | |
Posts: 5225 Rating:
|
Look at Network1 above. As for Network2... the "SPBNB" jump function I do not recognise. See if you can find out what it is for. w Late note: See [LINK] |
Last edited by: William_B at: 3/24/2015 6:51:26 AM |
|
3/24/2015 9:55 AM | |
Posts: 19 Rating:
|
Hello William_B,
Thank you very much for your inputs. I would be able to convert 1st network to LAD. But 2nd network I could not. Incase if you have any other idea please share with me. Thanks & Regards, Saidulu |
Last edited by: Sai442 at: 3/24/2015 9:57:34 AM |
|
3/24/2015 10:10 AM | |
Posts: 19 Rating:
|
Hello Hamid Hosseini, Your explanation is very useful for me and I am able to convert 1st network to LAD. Where as 2nd network I could not. There are few more networks are available to convert but I am facing problems due to lack of knowledge on STL. Here I am attaching Archived program backup, please help me. It has FB200, FC200, FC201 written in STL. In FB 200, except 2 networks others are converted to LAD using direct conversion option in Simatic Manager. In FC200 & FC201 most of the networks are not converting to LAD. This backup is created in SIMATIC MANAGER V5.5 SP3. It is very important for me. So need your help. Thanks & Regards, Saidulu
AttachmentBackup_program.zip (762 Downloads) |
Last edited by: Sai442 at: 3/24/2015 10:13:27 AM |
|
Follow us on