12/4/2013 5:22 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Program is saved in MMC (EPROM) for 300 and 400. Regards Manmeet
|
12/4/2013 5:31 AM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365)
|
Hello, Please, check the following FAQs for memory concepts for different produts (S7-300, S7-400): How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? How can I get an overview of the S7-400 memory concept? For S7-400, 2 types of memory cards (FLASH/RAM) are available.For temporary commissioning period, it is recommended to use RAM cards while for long-term retention of user program Flash card can be used.Read the following FAQ for more help regarding manipulation of Flash memory cards for S7 400. How can you write the program to the FLASH Memory Card when using a SIMATIC S7-400 CPU?As shown here, while downloading program is transferred to internal RAM memory of CPU.Transfer of data to external flash card is possible via PG or by using "save to memory card" from STEP 7. Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 12/4/2013 5:39 AM |
|
This contribution was helpful to2 thankful Users |
1/24/2014 10:15 AM | |
Joined: 8/19/2013 Last visit: 8/14/2024 Posts: 148 Rating: (10) |
absolutely correct ! How could i miss that thought ... |
3/26/2014 8:35 AM | |
Posts: 340 Rating: (6) |
new question is splittet to CPU S7-315-2DP, CAN I REPLACE IT BY S7-400 FLASH EPROM CARD |
Follow us on