9/17/2020 2:44 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
Here's the example. However, the storage of the values is not protected against power failure. If you need this, MAX/MIN blocks can be added.
AttachmentStore_counter_values_0BA8.Standard.zip (107 Downloads) |
This contribution was helpful to1 thankful Users |
9/17/2020 3:17 PM | |
Joined: 2/7/2017 Last visit: 4/11/2022 Posts: 92 Rating: (0) |
thanks for the info. Is it like this with the min/max to save the data? |
9/17/2020 3:24 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
Yes, correct. Mode 3 and REM = On. |
Follow us on