11/25/2009 10:51 PM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating: (20) |
Hi dear members and experts I will try to explain my problem. I'm changing some blocks in a project; i have 2 files; the first one is the original backup project and has not been changed; and the second one is the same project but with modifications, in the attachedscreen shot i'm showing a network in wich i make a comparision of integers;in the left side I'm showing the original FC160 andnetwork 21; and in the right side i show the same FC160with some modifications in diferent networks (I have not touched network 21 in this modified FC); as you can see the editor do not acept the parameter for the modifiedFC (this is "DB67.DBW86").DB67 is an instance DBandDBW86 it's declared as Word data type. Question is Why in the original projecti do not have an error, and Why in the modified project i have it?. I have to say thati have not modified network 21 in both projects i just made some other modifications in other networks in the modified project and the i make a "Check and update Accesses" and then when i try to save the modified FC the error apears. BTW, i have alredy comapredDB67 from original project VS modified project and time stamps are the same, also initial values and every thing else. Thanks all you for your help; have a nice day. AttachmentScreenshot_FC160.pdf (88 Downloads) |
Last edited by: TEBANCH at: 11/25/2009 10:56 PMKeep working! |
|
11/25/2009 11:09 PM | |
Joined: 10/7/2005 Last visit: 9/12/2024 Posts: 3020 Rating: (1054)
|
Hello TEBANCH Open any Block, select "Customize" from the "Options" drop down menu,untick "Type check of Addresses" as shown in the attachment and your problems shall go away (I hope). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on