3/8/2023 4:43 PM | |
Joined: 11/20/2012 Last visit: 10/31/2024 Posts: 8 Rating: (0) |
I am with the same problem. Tarciso. |
3/14/2023 8:12 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
Comparing https://docs.strongswan.org/docs/5.9/install/kernelModules.html to the kernel config, it seems some features are still missing there. Would need a patch against https://github.com/siemens/meta-iot2050/blob/master/recipes-kernel/linux/files/iot2050_defconfig_extra.cfg to enable those. Would you be able to build own images? |
This contribution was helpful to1 thankful Users |
3/20/2023 8:48 PM | |
Joined: 12/16/2019 Last visit: 10/10/2024 Posts: 4 Rating: (0) |
Thanks for the answer. Both libs were already installed. It is still not working after this new build. Attachmentmyvpn.txt (494 Downloads) |
3/21/2023 5:14 PM | |
Joined: 12/16/2019 Last visit: 10/10/2024 Posts: 4 Rating: (0) |
Thank you, jan-k. It is working now. |
Follow us on