8/2/2024 6:15 AM | |
Joined: 12/18/2014 Last visit: 9/8/2024 Posts: 33718 Rating:
|
You have to define more precisely what you want to do. Give more informations. |
8/2/2024 6:28 AM | |
Joined: 12/18/2014 Last visit: 9/8/2024 Posts: 33718 Rating:
|
Which computer? A normal PC or a Laptop? |
8/2/2024 6:31 AM | |
Joined: 8/2/2024 Last visit: 8/12/2024 Posts: 11 Rating:
|
I want it to work for both PC and laptop. |
8/2/2024 6:33 AM | |
Joined: 12/18/2014 Last visit: 9/8/2024 Posts: 33718 Rating:
|
And both can Modbus TCP/IP? |
8/2/2024 6:35 AM | |
Joined: 8/2/2024 Last visit: 8/12/2024 Posts: 11 Rating:
|
Yes, both can support Modbus TCP/IP |
8/2/2024 6:37 AM | |
Joined: 12/18/2014 Last visit: 9/8/2024 Posts: 33718 Rating:
|
Sorry, then I can't help you. It's new to me that a PC or a Laptop can be a Modbus TCP/IP slave. |
8/2/2024 6:47 AM | |
Joined: 12/18/2014 Last visit: 9/8/2024 Posts: 33718 Rating:
|
Why so complicated? Use the integrated web server of the LOGO!. |
Follow us on