7/18/2023 12:26 PM | |
Joined: 8/29/2022 Last visit: 7/18/2023 Posts: 1 Rating:
|
At one of our sites, we have PAC3220 multifunction meter and SICAM-T Transducer (7KG9661-1FA10-1AA0; PHOTO ATTACHED FOR YOUR REFERENCE). Both the instruments are mounted on 11KV VCB for 5MW motor. Also attaching The wiring schematic for your reference. Currently we are facing the issue where the power reading (KW) in PAC meter does not match with the KW reading in SICAM-T. Require your support on correct configuration to the attached wiring scheme. Attachment11KV ICOG Panel.pdf (223 Downloads) |
Follow us on