4/1/2021 12:51 PM | |
Joined: 11/15/2012 Last visit: 3/7/2025 Posts: 9 Rating:
|
Hello everyone I have recently started using wincc uinified. i am trying to make a wincc unified pc software. the runtime works perfectly when I run it from the local machine while when I try from a client machine on the network (pc windows) the start menu appears correctly but after clicking on the "start your project" button a white screen appears and after a few seconds it appears the message SwacLogin is unavailable I have correctly installed the certificate on both the server and the client machine, in fact this tells me that the site is safe Where am I doing wrong? thank you all
|
4/1/2021 1:41 PM | |
Joined: 6/22/2017 Last visit: 3/7/2025 Posts: 421 Rating:
|
hi torefra, do you use a DNS or did you check the option, that the Identity provider is the ip-Address? See: https://support.industry.siemens.com/cs/ww/en/view/109777591 If that is not the case i would double check the windows features. Best regards |
4/1/2021 2:30 PM | |
Joined: 11/15/2012 Last visit: 3/7/2025 Posts: 9 Rating:
|
thank you this FAQ solved the problem Was the DNS. but with the activation of the option "USE IP" works fine |
Last edited by: torefra at: 04/01/2021 14:31:40 |
|
This contribution was helpful to
1 thankful Users |
Follow us on