3/31/2020 8:42 AM | |
Posts: 46 Rating: (0) |
Hi, Where did you find the swimming pool sample project, i can not find any link on the Siemens Logo website Thanks a lot ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/31/2020 08:57:44New subject after splitting |
|
3/31/2020 8:47 AM | |
Joined: 12/18/2014 Last visit: 9/17/2024 Posts: 33779 Rating: (4194)
|
You find it in the download of the LOGO! Web Editor. The Download of the LOGO! Web Editor you can find here: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) This is a 1,3 GB sized complete package... |
3/31/2020 9:09 AM | |
Posts: 46 Rating: (0) |
Thanks for the fast reply, i have the download but i dont see the file for the pool project |
3/31/2020 9:16 AM | |
Posts: 46 Rating: (0) |
I have this sp1, but i dont see the file with the pool project |
3/31/2020 9:30 AM | |
Posts: 46 Rating: (0) |
Sorry, but ther must be a misunderstanding. When i download LOGO_V8_2_SP1_complete.zip there is no sample file. Something changed ? |
3/31/2020 9:50 AM | |
Joined: 12/18/2014 Last visit: 9/17/2024 Posts: 33779 Rating: (4194)
|
In this complete package is one part the software LOGO! Web Editor V1.0.1. If you unzipped the download of complete package, you have a folder "LOGO V8_2 SP1 complete". In this folder are two folders: In the folder "LSC_V8_2_SP1 Upgrade" are also two folders: In the folder "LWE_V1_SP1-Installer" are 3 folders.... (bla bla bla). It is too difficult for me to explain all of this to you. It's easier, I upload the sample project ... AttachmentSample.zip (265 Downloads) |
3/31/2020 10:16 AM | |
Joined: 12/18/2014 Last visit: 9/17/2024 Posts: 33779 Rating: (4194)
|
Yes, and then have you to start one of this exe files. |
Follow us on