9/23/2013 8:29 AM | |
Posts: 567 Rating:
|
Hi, I don't know if this tool works with PCS 7 V8.0 ASIA. But on the dowload page there is a contact person. I think you should contact him to answer this question. AVC: You have to order the AVC by your Siemens sales partner. More information about the AVC you can find here http://support.automation.siemens.com/WW/view/en/28448132 |
9/24/2013 2:54 PM | |
Posts: 16 Rating:
|
Dear Ammy, I have tested and readaccording to the document"Configuration of Texts and Languages in SIMATIC PCS ", Its means that The PCS7 includes 2 differents versions European and Asian, The PCS7 can be switched languages depending on what version you have installed ,For example if you order the Asian version PCS7 Then you can switch language between Chinese and English, Now My project needs switch language betweenRussianand English. Can you give some advise and methods for implemented this issue? Thanks very much! |
9/25/2013 8:41 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello Chengyue, First Installed the Russian language Region & Language in the Control Panel, this will you will do if you have Windows 7 Ultimate, Then when your Project is over then only you should Start the Project language Conversion using the Text Lib. & Import Again. The Detail is already Explain in the FAQ I have Post in my last Thread. |
Ammy |
|
9/30/2013 4:24 PM | |
Joined: 11/4/2011 Last visit: 1/19/2025 Posts: 253 Rating:
|
Here is my solution. I'm not sure that it is what you need, but I hope it is Components in the attached archive are intended to organize switching between Russian and English languages in WinCC Runtime. This is my personal method and it works in two Projects: one on PCS7 v7.1 and one on pure WinCC v7.0. I believe it suits PCS7 v8.0 as well but I could not be sure because I've never used PCS7 v8.x. Also it has nothing to do with translations of the whole Runtime, it is only needed for the Runtime's Language Switcher. I've made it up because I had no complete solution for translating WinCC to Russian. There are three main steps of changes: 1. Replacing the functions Close Runtime.2. Replacements in GraCS folder Go to the Project folder GraCS.3. Editing the Language button in @Buttons12.pdl Open @Buttons12.pdl from your Project's GraCS folder. AttachmentWinCC Runtime. Change Language English-Russian.zip (490 Downloads) |
Last edited by: TerminalBuzz at: 9/30/2013 4:26 PMбублик |
|
This contribution was helpful to
2 thankful Users |
10/9/2013 9:29 AM | |
Posts: 16 Rating:
|
Dear TermianlBuzz, AttachmentIssue for PCS7 Switch language.pdf (429 Downloads) |
Follow us on