9/16/2014 10:18 AM | |
Joined: 12/12/2011 Last visit: 7/9/2024 Posts: 69 Rating:
|
Dear Expert, i am doing project SIMOTION control. The system use C240 control 2 CU320 via profibus. After wiried cable, i did fast commisioning by Control Panel. but can not run Motor. i pop up alarm " the switch-on disable of the drive is active!" where i can fix it as well. Please give me advice. Thank You!
AttachmentControlpanelcommisioning.zip (429 Downloads) |
9/17/2014 5:46 AM | |
Joined: 12/12/2011 Last visit: 7/9/2024 Posts: 69 Rating:
|
Morning ChristophD, Thank you very much for your advice. while do commisioning control panel. have Fault "Motor Overcurrnent" and "motor blocked/speed controller at its limit". please how me where i can change Pramater limit matched. please help me clear this fault. Thank Advance!
AttachmentFault.zip (337 Downloads) |
9/17/2014 10:10 AM | |
Posts: 153 Rating:
|
Also check under Axis:Mechanics to see if you reversing the motor encoder. I had that before. |
4/4/2018 3:24 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by dipak123 is split to a separate thread with the subject Want to run S120 drive in Jog mode. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on