4/26/2013 8:54 AM | |
Joined: 6/4/2008 Last visit: 3/20/2023 Posts: 1419 Rating:
|
Hi, P0491 = 1. Automatic switchover to Encoderless in event of encoder fault.
Regards, Graeme |
4/26/2013 5:34 PM | |
Posts: 13 Rating:
|
Thank you |
5/6/2013 7:43 AM | |
Posts: 13 Rating:
|
Hi The Error code is F31131 we are using encoder for Hoist application. Thanks and Regards, Deepanraj.R
|
5/7/2013 9:43 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Hello, this error could be configured as warning for example - see http://support.automation.siemens.com/WW/view/en/68041075 or you configure your encoder without zero pulse. Why you use an absolute encoder where you want to work sensorless! Absolute encoder: When cyclically reading the absolute position, an excessively high difference to the incremental position was detected. The absolute position that was read is rejected. Limit value for the deviation: - EnDat encoder: Is supplied from the encoder and is a minimum of 2 quadrants (e.g. EQI 1325 > 2 quadrants, EQN 1325 > 50 quadrants). - other encoders: 15 pulses = 60 quadrants. Incremental encoder: When the zero pulse is passed, a deviation in the incremental position was detected. For equidistant zero marks, the following applies: - The first zero mark passed supplies the reference point for all subsequent checks. The other zero marks must have n times the distance referred to the first zero mark. For distance-coded zero marks, the following applies: - the first zero mark pair supplies the reference point for all subsequent checks. The other zero mark pairs must have the expected distance to the first zero mark pair. Fault value (r0949, interpret decimal): Deviation in quadrants (1 pulse = 4 quadrants). See also: p0491 (Motor encoder fault response ENCODER) Remedy: - check that the encoder cables are routed in compliance with EMC.- check the plug connections - replace the encoder or encoder cable - check whether the coding disk is dirty or there are strong ambient magnetic fields. - adapt the parameter for the clearance between zero marks (p0425). - if message output above speed threshold, reduce filter time if necessary (p0438). Zako |
Last edited by: zako_ at: 5/7/2013 9:47 PM |
|
Follow us on