5/16/2023 3:48 PM | |
Joined: 12/28/2016 Last visit: 2/26/2025 Posts: 435 Rating:
|
HiFiguren To increase the space between the content in the Symbolic IO-Field in WinCC Unified Systems, you can try using the following steps: 1. Right-click on the Symbolic IO-Field and select "Properties". 2. In the Properties dialog box, click on the "Content" tab. 3. Under "Content", click on the "Spacing" dropdown menu and select "Custom". 4. Adjust the values for "Spacing Before" and "Spacing After" as desired to increase the space between the content. 5. Click "OK" to apply the changes. If adjusting the spacing does not work for you, you may also try adjusting the font size or using a different font style to create more visual separation between the different indexes. Additionally, consider using grouping or other layout options to organize your content in a clearer way.
|
https://pnap.ir |
|
This contribution was helpful to
1 thankful Users |
Follow us on