7/29/2016 6:56 PM | |
Posts: 56 Rating:
|
My problem: convert 0-4 kHz to 0 -10V in Logo. |
7/29/2016 7:25 PM | |
Joined: 12/18/2014 Last visit: 6/29/2024 Posts: 33258 Rating:
|
Here is a possible solution. This is only a logo, which features fast counter, for example, the Logo 0BA8 12/24 RCE. Because then you can use the fast counter inputs I3-I6. AttachmentConverting_frequence_to_0-10V.zip (245 Downloads) |
7/30/2016 4:49 PM | |
Joined: 12/27/2006 Last visit: 6/6/2024 Posts: 1197 Rating:
|
this littele programm makes of a 0 - 4000 Hz input a 0 - 10 Volt signal. Proberly I3, I4, I5 or I6 I cant test it if its works good! Attachmentana-frekw2.zip (209 Downloads) |
Follow us on